3/28/2024 4:59 PM | |
Joined: 2/10/2015 Last visit: 8/21/2024 Posts: 288 Rating:
|
hi sir SANCRUZ, attash file for my online screen, I etablished connection with tia V15.1 |
3/28/2024 5:04 PM | |
Joined: 2/10/2015 Last visit: 8/21/2024 Posts: 288 Rating:
|
ONLINE AND DIGNOSTIC SCREEN |
4/9/2024 4:33 PM | |
Joined: 2/10/2015 Last visit: 8/21/2024 Posts: 288 Rating:
|
Hi 0_EINSTEIN, I created a new project under TIA V15.1 with the reference of the PLC CPU 1215C DC/DC/DC; 215-1AG40-0XB0 with latest version V4.3 I right-clicked on the configured PLC 1215C DCDCDC then I clicked on online and diagnostic but I cannot access the PLC, there is an error. see attached file including image FILE1 for the error. I again right-clicked on the configured PLC 1215C DCDCDC then I clicked on online connection but I cannot access the PLC, there is still the same error. see attached file including SCREEN1 image for error On the other hand, I created a project called 'test' without inserting the PLC reference then I clicked ONLINE and then LOAD DEVICE AS NEW STATION (HARDWARE AND SOFTWARE). At the moment I detected the CPU 1215C DCDCDC and the DISPLAY in the network, but when I clicked on LOAD in order to load the hardware and software configuration of the PLC, I saw the following error: Action interrupted before charging the device. see attached file including SCREEN2 and SCREEN3 images for error images. My apologies for the delay in my feedback, I was a little rushed in the last few days. THANKS . AttachmentFILE.zip (134 Downloads) |
Last edited by: Jen_Moderator at: 04/10/2024 07:53:35Text formatting optimized. |
|
Follow us on