2/20/2013 1:07 PM | |
Joined: 3/21/2006 Last visit: 10/1/2024 Posts: 10229 Rating: (1181)
|
You will need CP441-2 with the order numbers below:
One will be Master and the other Slave. For Master you need to buy6ES7870-1AA01-0YA1 and for Slave6ES7870-1AB01-0YA1 (hardware dongle). Physically both dongles are the same. The loadable driver Modbus Master (RTU) for CP441-2 is available for downloading in Entry ID:27774018. The loadable driver Modbus Slave (RTU) for CP341 and CP441-2 is available for downloading in Entry ID:27774276. |
This contribution was helpful to2 thankful Users |
2/26/2013 9:03 PM | |
Joined: 6/20/2011 Last visit: 9/13/2024 Posts: 27 Rating: (0) |
thx my friend ... what is correct mothod for ModBus for standard redundancy in S7-400H ? |
Follow us on