9/2/2008 9:08 AM | |
Posts: 15 Rating: (0) |
Hi Colleagues Does anybody know can i use et200l and et200b together with CPU315 2dp? Is theremake a problem or are they working on good condition? |
9/2/2008 9:40 AM | |
Posts: 487 Rating: (36) |
Hi If you can find the slave in the hardware list then you can use it Eric |
9/2/2008 9:56 AM | |
Joined: 5/28/2008 Last visit: 8/6/2024 Posts: 4515 Rating: (838) |
Hi GenghisKhan, Actually there's no problem to connect the ET200 L, ET200M, and ET200B together in the same profibus network using CPU315-2DP. Here's under a link shows that Siemens training center SITRAIN have a training kit "profibus simulator system 6ZB2500AA00". This unit a self contained control system with various PROFIBUS components and connections. Included is a S7315-2DP CPU and power supply connected via PROFIBUS to and ET200B, ET200M, ET200L-SC and to a S7342-5 PROFIBUS interface module. Explore the variety and power of Siemens remote I/O and PROFIBUS networking power with this packaged networking simulator system. |
Ayman Elotaify |
|
9/20/2008 5:23 PM | |
Joined: 1/17/2006 Last visit: 7/4/2024 Posts: 553 Rating: (29) |
Ithink ET220L has the transmission baudratelimited by 1.5Mbps andET200B can works until 12Mbps. So your profibus network transmission rate is limited by the lower component. see ET200L 32DItechnical data: https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&lang=en&objid=6ES7131-1BL10-0XB0&caller=view regards |
Last edited by: Berg at: 9/20/2008 5:26 PM"Educate the children and it won't be necessary to punish the men." |
|
Follow us on