3/26/2017 11:18 AM | |
Joined: 12/22/2006 Last visit: 1/25/2022 Posts: 1742 Rating: (309) |
Hello, You should not have more than x jobs active at the same time (where x depends on the CPU). In the system manual of the 1500 (V2.0), chapter 7.3 (asynchronous instructions) , you can read: If the maximum number of simultaneously running jobs for an instruction is exceeded, the instruction returns error code 80C3 (lack of resources) in the STATUS block parameter. The execution of the job is stopped until a resource becomes free again. |
Best regards |
|
Follow us on