1/13/2017 11:51 AM | |
Posts: 8 Rating: (1) |
Hello I am using the ET200SP on Simatic Step 7 v5.5, and I have two problems Problem 1: an AI card is not on the three of the ET200SP configuration When I go on the Configuration Manager to select the module under "Profibus DP > ET200 SP" then I have three options: V1.1, V3.0, and V3.1. On the module it says that it is V3.1.1 so I select V3.1 on the config manager. However I have an analog input card 6E67 134-6GB00-0BA1 which is not available for selection. So I am forced to use another product family. Problem 2: when using a different ET200SP, I get an error If I select a different ET200SP from "Profibus DP > Additional field devices > I/O > ET200 SP" then I have the possibility to add my analog card, but then I get a "Parameter error" for each group of cards. I tried to install revision 3 of the gsd file from here, but it doesn't change the error. I attach the config files and the error messages. Profibus module 100 is using rev 3, and module 125 is using rev 5. The error screens are here http://imgur.com/a/mwwmo Attachmentsimatic 300.zip (66 Downloads) |
1/13/2017 12:33 PM | |
Posts: 8 Rating: (1) |
I tried with a simple configuration (just PLC and ET200SP with cards) and the problem persists. I have attached the config file. Any idea?Attachmentsimatic 300_simple.zip (59 Downloads) |
Follow us on