9/17/2009 9:36 AM | |
Joined: 5/12/2006 Last visit: 8/8/2024 Posts: 22338 Rating: (3000)
|
Hello, following our experiencewith self constructed cables (reported by our colleagues and customers): - self constructed cables lead increased to problems,some of them are even sporadical, so they only occur after the machine is already running for a long time (quite hard to find..) - faults which were caused by self constructed cables are don't covered by the warranty! - the follow up costs in case of a faultare a lot more than the costs forbuying the original cable.. from the Thread: /tf/WW/en/Posts/19180 |
9/17/2009 4:19 PM | |
Posts: 133 Rating: (13) |
Although not recommended from the factory for the reasons stated if you have to make your own Drive CLiQ Motion Connect (green) cable connections between motor and drive I would cut the drive end and not the motor end. The motor end is a IP67/68 connector and is more complicated to replace. The drive end is a IP20 end and the metal cover can be reused. The RJ45 connector requires parts and tools supplied by Yamaichi. See yamaichi site for details but would only recommend doing this as last resort. http://www.yamaichi.com/ |
9/18/2009 4:28 PM | |
Joined: 3/2/2007 Last visit: 7/26/2024 Posts: 932 Rating: (5) |
Even if we use industrial shielded ethernet cables (STP)? Thank you |
... thank you ... |
|
Follow us on