10/10/2012 4:37 PM | |
Posts: 139 Rating: (1) |
Hello, colleagues! If I want use tranfer to panel through USB Host-To-Host cable I have to use exclusive driver from Siemens, as I can see here. But when I plug USB Host-To-Host cable to the port, Windows automatically install system driver (version 5.1.2600.0). When I try to Update system driver by way Disk\CD_3\Support\DeviceDriver\USB\WinXP, I have system message that in this folder are not appropriate or better driver. Does USB Host-To-Host cable work with system driver or how I can update system driver? Best regards, SpKV. |
10/11/2012 1:37 PM | |
Posts: 3037 Rating: (192)
|
Hello SpKV, You need one of these tested USB cable which you find in this FAQ. How can you transfer data via USB from a WinCC flexible configuration computer to a Windows-based operator panel and which USB cables can be used for this? Youuse another USB cable for the download, the download does not work. The best way is, you use the download about Ethernet or Profisbus. One of this works at each panel. Tweety |
10/12/2012 3:27 PM | |
Posts: 139 Rating: (1) |
Today I try connect to the OP270 panel with "Gembrid" USB Host-To-Host cable. It is really do not work. Best regards, SpKV. |
10/15/2012 11:19 AM | |
Posts: 3037 Rating: (192)
|
Hello SpKV, This cable is not tested for the USB driver. You want download your panel about USB, then you need these tested cable of the link. How can you transfer data via USB from a WinCC flexible configuration computer to a Windows-based operator panel and which USB cables can be used for this? Tweety |
10/15/2012 11:55 AM | |
Posts: 139 Rating: (1) |
Thank you, Tweety. Now I've understood. |
2/20/2013 2:47 PM | |
Posts: 3037 Rating: (192)
|
Hello, Do you use exactly this black cable of Belkin which you see in the document of site 5? Belkin Easy Transfer with item numberF5U258ea How can you transfer data via USB from a WinCC flexible configuration computer to a Windows-based operator panel and which USB cables can be used for this? Tweety |
Follow us on