1/6/2017 11:28 AM | |
Joined: 11/4/2015 Last visit: 12/12/2018 Posts: 7 Rating: (0) |
I'm using OPC UA version 8.1 with Windows 7 64 Bits SP1. I have two main problems when i usit it. FIRST PROBLEM : I have written a C# application and I use the dll’s that Siemens put on the web, where I have 1 Session connected to 1 PLC. I have1 group (or subscription) with 2 items that monitor. In another words if I have 1 item in two subscriptions after one receives an event after the PLC data change in the variable the item in PLC will not receive an event but two events, because I have two subscriptions. When in the past i used OPC DA I had two groups
I never had problems ilke this in OPC DA SECOND PROBLEM : Sometimes the bits in the PLC stays at 1 (integer) or True (Boolean) forever. I have had to do some software in the PLC so the PLC detects that a bit is a True more than 2 seconds, then the PLC put a False for 500ms and the put at True again. I didn't have that problem when i programed in OPC DA architecture, this problem arises when i change to UA architecture. I have a Cycle time in the OPC of 100ms. My Cycle when i create the subscription is a value of 100 (integer that represents 100ms) and the cycle to monitor the item is 100ms. See the pictures AttachmentPhotos.zip (33 Downloads) |
1/11/2017 6:10 PM | |
Posts: 1 Rating: (0) |
Hi Murof, I use OPC NET 8.1 with Windows 7 64 SP1. My communication is throe TCP/IP (Ethernet). The communication is using OPC UA. See the zip file in link bellow (The communication OPC – PC is throe DB1 of each PLC) https://www.dropbox.com/s/illmb7jkvczl4hi/Prf_Siemens.zip?dl=0 The DLL’s I take from Simatic example Programming an OPC UA .NET Client with C# for the SIMATIC NET OPC UA Server. In this link The DLL’s the I use are in the link bellow. https://www.dropbox.com/s/d4rquyspg2oc605/Api_OpcUA.rar?dl=0 The only modifications that I done was: Change the name of files Change the code in authentication so I can use the endpoint with(NONE | NONE)instead of(Sign and encode | Basic128RSA15) the change was in CertificateValidator_CertificateValidation I can send to you a sample project if you want with PC, please send me your email if you want so I can send you a wetransfer link so you can download. To answer to your questions that you put in another user topic. - Which OPC Server do you use? – OPC Server 8.1 - How is your Network configuration? It’s throe tcp/ip - Is the OPC Server on the same Computer as the Client? Yes - Which PLC do you use`? I used a CPU 317-2 PN/DP - if you use a S71200/1500 PLC, do you use optimized block access? NO |
1/12/2017 6:01 PM | |
Joined: 10/1/2013 Last visit: 5/8/2024 Posts: 605 Rating: (71) |
Hi rui,
Your example and this one are using the open source .NET stack from the OPC foundation (in different versions). If you want the news DLLs to work with you could check out the GIT repository of the OPC foundation: /Edit: Though I'm not sure if your problem is due to you client or the opc server. |
Last edited by: Owei at: 1/12/2017 6:01:35 PMLast edited by: Owei at: 1/12/2017 6:05:25 PM |
|
Follow us on