5/23/2017 3:35 PM | |
Posts: 9 Rating: (0) |
Dear all, Can you help me , i using S7400 , wich fb or fc i can use for incremental encoder? Thank! ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 5/24/2017 12:02:55 PMNew subject after splitting |
|
5/28/2017 3:55 PM | |
Posts: 9 Rating: (0) |
Hi, i am using IM 153- 2 = 6ES7 153-2BA02-0XB0 and FM350 COUNTER-1 = 6ES7-350-1AH03-0AE0 |
Last edited by: Antony_BR at: 5/28/2017 4:01:19 PM |
|
5/28/2017 4:16 PM | |
Joined: 9/27/2006 Last visit: 7/6/2024 Posts: 12267 Rating: (2675)
|
Hello Anthony; These documents should give you the information you need: SIMATIC FM 350-1 First Steps in Commissioning Integrating into the User Program Open the library FMx50LIB in the SIMATIC Manager using the menu commandFile > Open...Libraries. Copy the functions FC 2 and FC 1 and the user-defined data type UDT 1 from the“Blocks”container of the FMx50LIB library to the “Blocks” container of your project. Insert DB 1 as DB with data type UDT 1 into the “Blocks” container using the menu command Insert > S7 Block > Data Block. Open the popup menu in HW Config by clicking with the right mouse button on the FM 350-1 entry. sing theObject Propertiesmenu command start theProperties – FM350-1 COUNTERscreen form. Using theMod Addr...button you can now automatically enter the module address (MOD_ADR) (in the example: 256 corresponds to 100 Hex), the channel address (CH-ADR) and the channel length set underAddressesin the channel data block. Also: FM 350-1 Counter Function Module Installation and Parameter Assignment Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 5/28/2017 7:31:23 PM |
|
5/28/2017 7:10 PM | |
Posts: 9 Rating: (0) |
I can not find this FC , how i can update the libery? thans for your help. |
5/28/2017 7:51 PM | |
Joined: 9/27/2006 Last visit: 7/6/2024 Posts: 12267 Rating: (2675)
|
Hello Anthony; Sorry, I presumed you would have the application CD that contains the configuration software for the FM 350-1; it was delivered along with the function module. Here are links to different items contained in the configuration CD; the FM Configuration package should be required only if the FM 350-1 Configuration Software complains about any installation issues. Configuration Software for FM 350-1 and FM 450-1 Counter Modules FM 350-1 Block program (App# 225) Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 5/29/2017 4:19:48 PM |
|
This contribution was helpful to1 thankful Users |
5/29/2017 3:29 PM | |
Posts: 9 Rating: (0) |
Hello Daniel, Thank you very much really help a lot. |
Follow us on