6/22/2012 3:51 PM | |
Posts: 21 Rating: (1) |
Good Morning, I created my 5th FB in my project with one rung of logic and when I call it as the first block in OB1 download it, it is green on the EN but the ENO is red (See attachment). When I move the call to anywhere else as long as it's not called first, it works and both EN and ENO are green as they should be. I am scratching my head on this one on why it matters where it is called.... Thanks for your help, Jason
AttachmentFB_BROKE.zip (59 Downloads) |
6/22/2012 4:32 PM | |
Joined: 1/28/2009 Last visit: 9/10/2024 Posts: 6849 Rating: (1365)
|
Hello OUFAN75, Attachment explain a bit your case with reconstructed case.I manipulate BR with "#br_manual" input parameter. [code] CLR A #in1 A #in2 = #aus A #br_manual SAVE [/code] Hope this helps Best regards Hamid Hosseini AttachmentBR.zip (57 Downloads) |
Last edited by: hdhosseini at: 05/30/2019 23:10:24 |
|
6/22/2012 6:37 PM | |
Joined: 10/7/2005 Last visit: 9/16/2024 Posts: 3020 Rating: (1054)
|
Hello OUFAN75 have alook at the following two threads,they'll hopefully contain the answers to your questions: Online Laddder - Dashed FB call Regarding the BR bit |
Cheers |
|
This contribution was helpful to3 thankful Users |
6/22/2012 6:40 PM | |
Joined: 1/28/2009 Last visit: 9/10/2024 Posts: 6849 Rating: (1365)
|
Hello again, All you needed provided in the attachment.But, I think some complementary explanation is necessary! 1-BR is one of the status bits in CPU and used to implement EN/ENO mechanism.There are some useful posts in the forum you can search for.It is used as an indication for user of a function or a function block that execution of that done without any error in CPU.It is also applicable for System functions.Normally BR is set to "TRUE" in the beginning of a block and It is important for developer of a function to reset it in case of any error such as range violation in calculation, illegal floating point number,illegal input for arithmetic functions and ... . 2-So, in your case, As we can not see what you have done in your FB, I guess you never set "BR" and it is "FALSE" when function execution ends and you face the frightening red line.Simply, to avoid that, at least add following codes in your FB. [code] SET SAVE [/code] Thank you "fritz" for providing all related topics.I clustered all in the following TAG: Cases on BR-EN/ENO Mechanism Best regards Hamid Hosseini |
Last edited by: hdhosseini at: 6/22/2012 6:48 PMLast edited by: hdhosseini at: 05/30/2019 23:10:47 |
|
This contribution was helpful to3 thankful Users |
6/22/2012 7:32 PM | |
Posts: 21 Rating: (1) |
Thank you gentlemen for the detailed explanation |
Follow us on