Industry Online Support
Technical Forum
9/5/2008 7:55 AM | |
Posts: 139 Rating: (25) |
Hi did you have any luck troubleshootingthis one yet? |
9/5/2008 11:01 AM | |
Posts: 54 Rating: (0) |
Nope! still can't detect the printer being unplugged! |
9/5/2008 2:56 PM | |||||||||
Posts: 487 Rating: (45) |
Just curious about the paramaterization
Have you set this paramater as Yes? |
||||||||
9/5/2008 3:12 PM | |
Posts: 54 Rating: (0) |
Hi Yes I saw this and thought thats what I need on, but didnt make any difference! (see my 1st post) |
Last edited by: G_H at: 9/5/2008 3:13 PM |
|
9/5/2008 3:28 PM | |
Posts: 487 Rating: (45) |
Also are you using 8 wire cable or just 3 wires, you need to have all the signals used so that these signal states can be checked. I think you need to select flow control RTS/CTS on both side and also use S_VSTAT and S_VSET. Have you tried with these? The following faqs also may be handy http://support.automation.siemens.com/WW/view/en/25358470 http://support.automation.siemens.com/WW/view/en/21363754 |
9/5/2008 3:34 PM | |
Posts: 54 Rating: (0) |
thanks Jomy, the problem now is the system is shipped to site so harder for me to play with it! will check all this next site visit. cheers |
Follow us on