1/24/2006 3:38 PM | |
Posts: 1084 Rating:
|
[quote user="ranr_mids"]I've been experimenting with your suggestions, and have hit one or two snags. First, I'm having trouble passing thequery I want to the Alarm Control. I need to assemble the query using script, as the query needs to be context-driven. Second, the query is not having the desired effect on the alarm list. Third, when I attempt to 'view' the query via the Alarm Control I get the following message: "The selection was changed in such a manner that it can no longer be displayed in the Selection dialog. To open the dialog, the current selection must be discarded". First, You can not pass every query into the alarm control. for instance: You can not use "OR" in your query's (you should alter it in a way that you use LIKE. If you set a query to the control that he does not know OR the query is to complex (but still could work) you will get the message: "The selection was changed in such a manner that it can no longer be displayed in the Selection dialog. To open the dialog, the current selection must be discarded". Could you put your query into this thread, then I can have a look. also the way how you want to submit it to the control. with regards **** You can also have a look at the following FAQ: http://support.automation.siemens.com/WW/llisapi.dll/5668269?func=ll&objId=5668269&objAction=csView&csquery=msgfiltersql&foldersopen0=-184-769-&nodeid0=10805548&lang=en&siteid=cseus&aktprim=0 |
Last edited by: Ikkezelf at: 1/24/2006 3:42 PM |
|
Follow us on