8/1/2024 5:06 AM | |
Joined: 3/11/2019 Last visit: 9/6/2024 Posts: 1569 Rating:
|
Hi, for download, means transfer the program from PC to PLC, the firmware difference doesnt matter. How do you load a project into an S7-1200 CPU if its firmware version cannot be selected in the hardware catalog of STEP 7 (TIA Portal)?How do you load the project data if the version of the firmware installed in the S7-1500 CPU cannot be selected in the hardware catalog of your version of STEP 7 (TIA Portal)?
So If the program currently on the CPU was transfered with V15, you will also need V15 for the upload. If the program was transfered with V13, you can use V13 (Firmware doesnt matter). Within V13 there are additional dependencies with servicepacks. Check this FAQ. What options are available in STEP 7 (TIA Portal) for uploading when the project version in the CPU no longer matches the version on your PG/PC?regards sancruz |
Last edited by: sancruz at: 08/01/2024 05:10:59Feedback appreciated, please rate |
|
This contribution was helpful to
1 thankful Users |
Follow us on