5/23/2023 6:06 PM | |
Joined: 4/20/2023 Last visit: 8/19/2024 Posts: 33 Rating: (0) |
Yes, I know that they are edge-triggered. Do you mean if I keep the movement instruction inside the case, it will be triggered more than once? Sure the text file is attached here. thanks for the hint. AttachmentNew Text Document (2).txt (351 Downloads) |
7/13/2023 9:47 AM | |
Joined: 4/20/2023 Last visit: 8/19/2024 Posts: 33 Rating: (0) |
Hi again, Thanks for the answer. I just tested the program again. Only first movement of the program works once. It doesn't move to #step 1. Although the movement of previous axis is done It's not going through "Case ... OF ". I really appreciate for the help. The code that I used is in the text file. AttachmentNeues Textdokument (4).txt (310 Downloads) |
Follow us on