11/4/2016 12:26 PM | |
Posts: 1 Rating: (0) |
I simply need a way to force a specific DB number to name assignment on import. This is because the DB number needs to be exchanged for communications. It is not sufficient to determine it at runtime, it must be predetermined. So yes, it is certainly possible to never refer to such DBs with any name, but only by number, and write your own compiler to generate such code. However, is there a way to specify the DB number? Maybe like similar to DATA_BLOCK "my_db_send_data" Searching for import file syntax does not yield any complete-looking information, so there must be quite some undocumented features...? For any other use I can find block numbers at runtime if needed, but this does not work in the above mentioned case. ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 11/4/2016 1:14:27 PMNew subject after splitting |
|
Follow us on