2/29/2020 4:36 PM | |
Joined: 11/20/2017 Last visit: 11/14/2022 Posts: 6 Rating:
|
Dear Expert I have DC Motor 300KW / 440VDC / 740A / ( 650/1300RPM ) I use DT Configurator to configure size of Sinamic DCM drive, I have a question about amper rating for Fuse Armature DC is 3NE3334-0B, When i check the rating current for that fuse is 500 A. SITOR fuse link, with slotted blade contacts, NH2, In: 500 A, aR, Un AC: 1000 V, front indicator My question is this OK ? because my motor current is 740 A base on the Name plate, Or i have to change base on motor Data Thanks Regi Attachment6RA8087-6FV62-0AA0-Z_G00+G20+S01_datasheet_en.pdf (67 Downloads) |
3/11/2020 3:32 AM | |
Joined: 11/20/2017 Last visit: 11/14/2022 Posts: 6 Rating:
|
thanks sir |
Follow us on