11/3/2023 7:37 PM | |
Joined: 1/21/2013 Last visit: 4/18/2025 Posts: 3764 Rating:
|
Hi, I assume MAZENJER is talking about the LKinLang (SIMATIC S7-1500T Kinematics Language) library. Some years ago I was involved in a project where this library was used on a SIMATIC ET 200SP Open Controller. Unfortunately I was not responsible for the integration of the library, but as far as I remember it was necessary to transfer the files to the load memory using the integrated web server. However, using the "Provide feedback" link at the bottom of the page will help you get in touch with a person responsible for this library. This person may be able to answer your question. But do not forget to publish the answer here. Kind regards |
This contribution was helpful to
4 thankful Users |
Follow us on