11/6/2019 8:21 AM | |
Posts: 9 Rating: (0) |
The IOT2040 that I am working on has the same problem. Where I can only access the internet if my office Wi-Fi network provides IP address via dhcp. The moment I use a static IP address, I loose internet connection. Where the gateway cannot ping 8.8.8.8.
I have tried to follow the steps, to unlink resolv.conf, create a new resolv.conf with the following content, (which are the same content as when the dhcp assigns the dns into the resolv.conf file)
as well as, making /etc/resolv.conf immutable. by using
All the above steps didn't help resolve the problem. Are there things that I should look out for? like spaces, special characters, etc... ? Must I only use nano to edit the resolv.conf file? I also used Notepad++ to edit the file. Is there another file that I have to manually change if I'm using static IP via Wi-Fi? ------------------------------------------------------------------------------------------ |
Last edited by: ziml at: 11/06/2019 08:33:29Last edited by: Jen_Moderator at: 11/07/2019 08:24:13New subject after splitting |
|
11/10/2020 3:01 PM | |
Joined: 4/28/2015 Last visit: 6/3/2024 Posts: 3345 Rating: (379)
|
Hi, why is resolv.conf a folder in your case? That doesn't make sense.. It is since you tried to delete it create it again? Maybe the deletion was a wrong advice.. I meant unlink it, sorry. Here you can find the right instructions Best regards! |
Last edited by: bergmanu at: 11/10/2020 15:04:56Not working for IOT2050 support anymore from March 1st, 2024. |
|
Follow us on