10/10/2023 4:58 AM | |
Joined: 1/20/2022 Last visit: 7/13/2024 Posts: 9 Rating:
|
Dear all, Greetings of the day, My requirement is to Generate report for the System, Suggest me the Sollutions. I have 3 - 1500 and 4 - 1200 PLC using TIA with Wincc standalone server and I'm Communicating all the Wincc server to Historian and all the data will be Logged in Historian. Which also includes String Data Type But Historian unable to Store String data Type. mainly string data are Batch Name Customer required Batch name to be used as a Filter to generate Report. also we are Using one Wincc IO server which will act as a Overview for all the System. 1. I can Communicate all the Wincc server to Wincc IO server and I can make single Communication to Historian. but alarms time stamp are mismatching in that case. 2. if I'm Communicating all the Wincc server Directly unable to Store the String value int he Historian. Give me some recommendation on this Topic. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/10/2023 10:28:15New subject after splitting |
|
2/13/2024 1:51 PM | |
Joined: 1/20/2022 Last visit: 7/13/2024 Posts: 9 Rating:
|
Hi Murof, I'm using Wincc 8.0 with PHIS 2020 sp2 |
Last edited by: shehin at: 02/13/2024 13:52:42 |
|
Follow us on