12/18/2020 7:20 PM | |
Joined: 6/28/2019 Last visit: 6/10/2024 Posts: 2 Rating: (0) |
Hello All, I'm using tia portal v16 with an s7-1200 DC/DC/Relay PLC. I'm currently working on a project that uses 2 pumps in a lead lag configuration in which a report needs to be generated each day at 7am. The report would include the total flow from the day, pressure differentials, and the GPM when the flow is active. I have gone through different forum posts to try and determine how to generate this report at 7 am and I'm leaning towards using the RD_LOC_T function but do not understand how to specify the time I would like the report to be generated. I am also not sure if I have set up the report (which will be exported as a csv file) correctly. Is there some documentation on how to export a report as an excel file. I've gone through the help files to try and gain a better understanding of this process. Is there anyone who has experience doing this? If so can you provide any guidance to this novice programmer who is over his head right now?(me lol) Attached is my program as it currently stands. Username: admin Password Siemens1 Thanks in advance for the help. Happy Holidays, Andrew ps I had to take the HMI screens out of my project to be able to attach it here Attachment695830 East Mountain test without hmi screens.zip (73 Downloads) |
Follow us on