9/2/2015 11:14 AM | |
Joined: 5/12/2006 Last visit: 9/18/2024 Posts: 22358 Rating: (3011) |
Hello, if you open the properties of the device you can find the name of the used GSD file. Regards Christoph |
9/2/2015 11:15 AM | |
Joined: 1/28/2009 Last visit: 9/10/2024 Posts: 6849 Rating: (1365)
|
Dear User, In my project i have a profibus node which is having node number 4. but this node showing DP-NORM. For installing GSD file for this node i don't have details of the component. Is their any possibility to get the gsd file for unknown component. When a DP-Slave is shown with DP-Norm , it means there is not stored bitmap picture for that in STEP 7 database.There is only case that slave is shown with question mark (????) , the GSD file doesn't present in the database of your system.If you have the view like shown in attached file, simply click on the slave and the name of GSD is available to and you can find it in S7DATA folder. If GSD file is not available the slave is shown with question mark (????), you need to search the website of the manufacturer the exact version of hardware and download the GSD file and other supporting data. I hope that helps, hdhosseini AttachmentGSD.rar (332 Downloads) |
Last edited by: hdhosseini at: 9/2/2015 11:17:15 AMLast edited by: hdhosseini at: 9/2/2015 11:18:19 AM |
|
This contribution was helpful to1 thankful Users |
9/2/2015 11:23 AM | |
Joined: 8/31/2005 Last visit: 8/20/2024 Posts: 2198 Rating: (328)
|
A quich search for THDP0091.GSD brings this result: http://files.pepperl-fuchs.com/selector_files/navi/productInfo/doct/tdoct1184__eng.pdf So I think you have a "SPI3 PROFIBUS DP Slave" from Pepperl+Fuchs. |
|
|
9/2/2015 12:25 PM | |
Posts: 303 Rating: (3) |
thank you all for your responses. I tried with 'HIL_0C0E.GSD' but inable to figureit out, please share if any one have this gsd file. |
9/2/2015 1:46 PM | |
Joined: 1/28/2009 Last visit: 9/10/2024 Posts: 6849 Rating: (1365)
|
I tried with 'HIL_0C0E.GSD' but inable to figureit out, please share if any one have this gsd file. Check this: Gateway PROFIBUS DP Slave to Modbus RTUNT 100-DP-XX, NT 100-XX-DP PROFIBUS DP Slave GSD (Device description file) Attachmentgsd2.rar (247 Downloads) |
Last edited by: hdhosseini at: 9/2/2015 1:49:00 PM |
|
9/4/2015 2:33 PM | |
Posts: 303 Rating: (3) |
It worked, Thank you |
This contribution was helpful to2 thankful Users |
Follow us on