Industry Online Support
Technical Forum
1/1/2012 4:49 PM | |
Joined: 3/21/2006 Last visit: 7/26/2024 Posts: 10228 Rating:
|
Hello, In order to undesrstand what is the reason for that STOP load in CPUs some error's OBs. Which organization blocks do you need for error handling? Best regards, Hristo Mihalev |
1/1/2012 9:08 PM | |
Posts: 167 Rating:
|
Hi What does the diagnostic buffer say?
|
1/2/2012 6:31 AM | |
Joined: 2/5/2009 Last visit: 9/3/2024 Posts: 11 Rating:
|
Dear Belbra, I have used these Hart Modules & configured without any difficulty . Now it is working. Are you using secondary varibles from Hart module or only the Primary variable ( 4..20 mA) ???. Find the attachment. It may help you. Regards, AttachmentHartConfig.zip (282 Downloads) |
1/2/2012 7:05 AM | |
Joined: 3/21/2006 Last visit: 7/26/2024 Posts: 10228 Rating:
|
Did you receive any error during "Save and Compile" of hardware configuration? Of course after you should download it to the CPU. To mention (is not important) in order to use all functionalities of that analog module the preconditions are:
Best regards, Hristo Mihalev |
Follow us on