4/20/2017 4:07 PM | |
Posts: 3 Rating: (0) |
if i change CUVC board , i would like to ask about i must download parameters or no need to download parameters. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 4/21/2017 12:02:52 PMNew subject after splitting |
|
4/24/2017 4:03 PM | |
Joined: 10/11/2006 Last visit: 5/23/2024 Posts: 5852 Rating: (793)
|
Dear hfjkhsjhsj the parameters and power part settings are stored on the CUVC board. Hence changing the CUVC board requires a parameter download. Power part and parameterization please find section 6.3 in the detailed parameterization The link to the compendium Masterdrives VC 3.4:http://support.automation.siemens.com/WW/view/en/13472409 The link to the commissioning tool DriveMonitor:http://support.automation.siemens.com/WW/view/en/11769381 |
Last edited by: TechTeam at: 4/24/2017 4:04:13 PMLast edited by: TechTeam at: 4/24/2017 4:04:29 PMWith best regards, |
|
This contribution was helpful to1 thankful Users |
Follow us on