2/5/2017 12:21 AM | |
Joined: 11/7/2015 Last visit: 5/24/2024 Posts: 4 Rating:
|
In one of the program there is STL Statement Can you pls help me to understand IT L PIB [AR1,P#1.0] T DIB 47 L PIB [AR1,P#2.0] T DIB 48 L PIB [AR1,P#3.0] T DIB 49 L PIB [AR1,P#4.0] ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 2/6/2017 3:20:29 PMNew subject after splitting |
|
This contribution was helpful to
1 thankful Users |
2/6/2017 6:19 PM | |
Joined: 12/9/2010 Last visit: 10/8/2022 Posts: 623 Rating:
|
Hi Pramod26, This code section will move 3 bytes of PIB[peripheral input] to data byte 47 through 49 of OPENed Data block. The given info. is not sufficient to explain exactly the PIB no and DB no. There must be instructions LAR1 and OPN DB. U need to mention them here. |
If you like the comment, rate it (right top) or thank it (left bottom). |
|
This contribution was helpful to
1 thankful Users |
Follow us on