7/5/2013 8:46 AM | |
Joined: 10/3/2010 Last visit: 9/30/2024 Posts: 1562 Rating: (192) |
stumbled on this topic by accident, maybe have look at this No experience with it but might be worth a look? On the other hand, it's quite strange (at least for me) to look for a Siemens panel for doing complete Modbus Master/Slave communications. If a Siemens panel is not a must in this case, I would search for other brands, more specialized in Modbus protocols. |
Last edited by: SteBo at: 7/5/2013 8:53 AMB r g d s , |
|
This contribution was helpful to1 thankful Users |
7/5/2013 9:00 AM | |
Joined: 3/18/2008 Last visit: 12/8/2023 Posts: 1750 Rating: (272) |
Hello, I am not sure what could be the best third Party HMI to be choose for above requirement but in one of my project i used Sthal HMI. We have used it as modbus master in One of our Porject with S7200 PLC. For more details, you can visit here www.stahl-hmi.de/ |
Last edited by: Amit_86 at: 7/5/2013 9:01 AMVANDE MATARAM..... |
|
This contribution was helpful to1 thankful Users |
7/5/2013 9:41 AM | |
Joined: 1/21/2013 Last visit: 9/4/2024 Posts: 4620 Rating: (708) |
Hi SolutionFinder, I'd watch a converter from Ethernet to Modbus or what you want. Go to Anybus Fieldbus and Ethernet connectivity solutions from HMS ... |
This contribution was helpful to1 thankful Users |
7/5/2013 5:57 PM | |
Posts: 378 Rating: (73) |
Hello SolutionFinder, Here is my suggestion by considering your minimum price requirement: 1. HMI: - Any desktop PC that matches your memory requirement: ----- Estimated Price = $300 - LCD Monitor with screen resolution of 640X480 OR 800X600 OR 1024X768 OR 1280X1024 OR 1600X1200 OR 1440X900 OR 1680X1050 OR 1920X1080 OR 1920X1200 : ----- Estimated Price = $100 - USB Touch Screen Overlay: Google it or see this link http://www.cyclotouch.com.au/product_info.php?products_id=2501 : ----- Estimated Price = $140 - SIMATIC PC Adapter USB : ----- Estimated Price = $400 ----- ---------> Total Estimated Price = $940 2. Modbus: - Search for ModBus master/slave device have a look at this site http://www.hms.se/products/abc.shtml Now I hope you are satisfied with the HMI but you might have the following technical questions: How to program the modbus send/receive? Ø Install ModBus master server (I guess you will get the CD with modbus device) , then you can program it directly from WinCC script. 2. How to program HMI? and How HMI work? Ø Using WinCC flexible runtime as a device type and generate FWX file. On HMI PC install WinCC flexible runtime software with Automation license manager. Mount USB Touch Screen Overlay and install driver. Install SIMATIC PC Adapter USB driver and connect to your PLC. Ø How the user uses the program? You have to copy FWX file to some location and make it to automatically run during the boot (see my attachment on details). Hope helps and note that I have just done such kind of project except the modbus part and I have attached here this project thus extract to your desktop, run as administrator on Install.bat file and to exit press SHIFT five times. Regards, AttachmentProgram1024x768.zip (77 Downloads) |
Last edited by: desmul24 at: 7/5/2013 6:21 PM |
|
This contribution was helpful to1 thankful Users |
7/5/2013 9:47 PM | |
Posts: 559 Rating: (87) |
Dear All, Thanks a lot all for giving very quick & valuable replies I will think on that & go for some good solution. But surely I will share with you all guys.
|
1/14/2014 1:27 PM | |
Joined: 4/24/2009 Last visit: 8/20/2024 Posts: 2682 Rating: (135) |
New question splitted to communicate STAHL HMI (ET-306) with S7-1215 on profibus with CM1243-5?. Best regards O_Moderator |
Follow us on