Industry Online Support
Technical Forum
11/30/2011 8:39 AM | |
Posts: 165 Rating:
|
Dear expert and all I am facing the problem in HMI via ethernet connection. I have my laptop(PG/PC) , SIMOTION C 240, and HMI (MP 277 10" TOUCH)winCC flexible 2008. I have attached my hardware configuration in the form of screen chart.I could go online with my simotion controller from my pc through ethernet. but icant in HMI. Is it possible to acess the HMI from PC? PG/PC--- SIMOTION= ethernet SIMOTION--- HMI = profibus (12Mbps) Can i download or access HMI from my PC? Please help me (note: we could access the HMI and SIMOTION via profibus (by CP5512) and the node address are detected. we are trying to access the hmi via ethernet) Thanks Attachmenthardware_config.zip (477 Downloads) |
Last edited by: O_Moderator at: 11/30/2011 10:52 AMnew subject after splitting from /tf/WW/en/Posts/59629#top |
|
11/30/2011 5:32 PM | |
Posts: 3037 Rating:
|
Hello, Perhaps, this FAQ can help you? How do you use WinCC flexible to transfer a project to an operator panel via S7 routing? Tweety |
12/1/2011 8:36 AM | |
Joined: 5/12/2006 Last visit: 9/2/2024 Posts: 22350 Rating:
|
Hello, yes routing is avaiable for SIMOTION C240. You must assign a PG/PC on then ehternet Network and select the NIC which communicate with the C240. take a look on this thread /tf/WW/en/Posts/65156#top Regards Christoph |
12/2/2011 9:52 AM | |
Posts: 165 Rating:
|
Dear Expert Thanks for your valuable reply. I have one doubt in the above thread. where i should enable the router? either in PG/PC or SIMOTION ? should i give any IPaddress to myHMI? I have attached my ethernet settings with hardware configuration in word format. Please let me knowwhere i should change the settings to access the HMI from my PG/PC. PG/PC IP : 169.254.52.198 SIMOTION IP: 169.254.52.197 and MPI/DP address of HMI is: 21. I am using cross ethernet cable to connect simotion DP/MPI port and HMI. thank you Attachmentdetail_hardware_config.zip (302 Downloads) |
Last edited by: Mothilal at: 12/5/2011 7:28 AMLast edited by: Mothilal at: 12/2/2011 11:37 AM |
|
Follow us on