8/11/2023 12:40 PM | |
Joined: 4/11/2022 Last visit: 6/28/2024 Posts: 5 Rating:
|
i would like to ask for information too, since I have a problem with the homing of the Epos (and associated SinaPos). i want to make the homing via the reference mode (Mode = 4), but i don't understand WHERE to connect the cam reference sensor (an inductive sensor). on the G120 (CU250S) inverter on parameter p2162 is setup the following parameter r2092.2 CO/BO: PROFIdrive PZD3 receive bit-serial: Bit 2 that i can not change. In the SinaPos block i don't see any input where to put the digital input. i understand that i need to set the bit 2 of PZD3 ON when the machine is on the zero position sensor, but i see no obvious input on the sinapos. i think putting the EPosSTW2.%X2 value to TRUE would be useless, since the DPWR command is done inside the Sinapos, so my only option is setting TRUE the exact output AFTER the Sinapos command (like Q404.2 :=TRUE, assuming the telegram starts at QW400) i'm missing something? thank you in advance Mattia ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 08/14/2023 04:27:57New subject after splitting |
|
8/14/2023 11:36 AM | |
Joined: 10/11/2006 Last visit: 7/12/2024 Posts: 5874 Rating:
|
Hello Mattia, |
With best regards, |
|
Follow us on