1/9/2015 5:27 PM | |
Joined: 8/31/2005 Last visit: 10/22/2024 Posts: 2198 Rating: (328)
|
Can you export the diagnostic into a txt file and post here? Try to start the C7 PLC as described in chapter 2.2 in http://support.automation.siemens.com/WW/view/en/1135678/0 |
|
|
1/10/2015 11:20 AM | |
Posts: 24 Rating: (0) |
There is problem the screen mode of C7 Op is closed by password.i can not enter to operation mode screen |
1/29/2015 8:21 AM | |
Joined: 1/21/2013 Last visit: 10/23/2024 Posts: 4620 Rating: (708) |
Hello, maybe our friend vipz means this look the explanation of 24VDC (C7 Power Supply)Pin No. 3 and 4 Go to page 2-14: SIMATIC C7-623, C7-624 Control Systems Volume 1 ... - Siemens |
Last edited by: Ste39 at: 1/29/2015 8:23 AM |
|
1/29/2015 10:23 AM | |
Posts: 24 Rating: (0) |
Hi: In the manual there is no enaugh informations for authorization terminals 3 &4 did you have this infomations |
1/29/2015 10:35 AM | |
Joined: 9/2/2012 Last visit: 8/15/2024 Posts: 711 Rating: (30) |
HaiM.Alawini, Can you please tell the problem that you are facing ? Because initialy you mentioned that CPU is in stop because of internal error, now you posted as some password option.[you wrote--There is problem the screen mode of C7 Op is closed by password.i can not enter to operation mode screen]. so please let us know the actual problem and kind of help you are looking for..
|
|
|
Follow us on