7/10/2013 1:49 AM | |
Joined: 5/1/2013 Last visit: 7/28/2024 Posts: 427 Rating:
|
I am using wincc 7.0 I want backup wincc project. How can I backup project... Just copy the project folder? |
7/10/2013 3:41 AM | |
Joined: 9/27/2006 Last visit: 8/11/2024 Posts: 12275 Rating:
|
Hello RetroL; Use the WinCC Project duplicator; see the attached screencapture, taken from this manual: SIMATIC HMI WinCC V7.0 SP1 MDM - WinCC: Working with WinCC 1.10.2 How to Copy a Project
Introduction You can copy the configuration data and the runtime data of a closed project.
Principle Select the project you want to copy in the Project Duplicator. Enter the folder into which the project will be copied. In the description below, this folder is called the target folder. The target folder can be on the same computer or on another computer in the network for which you have access rights. The project folder is created in the target folder. When you copy it, you can change the name of the project. The project folder is created with the project name. You can only copy the entire project and the entire folder structure. You cannot exclude any data or folders from the copy operation. After the project has been copied, you can open and edit or activate it immediately. If you open the project on another computer, you must change the computer name. Hope this helps, |
This contribution was helpful to
7 thankful Users |
7/10/2013 7:06 AM | |
Joined: 3/18/2008 Last visit: 12/8/2023 Posts: 1750 Rating:
|
Hello, Apart from above information from Daniel, you can also take backup of WInCC Porject in Runtime... Have a look at here. How do you save/copy WinCC projects while WinCC Runtime is running? Hope this helps. |
VANDE MATARAM..... |
|
This contribution was helpful to
3 thankful Users |
7/10/2013 7:28 AM | |
Joined: 10/3/2010 Last visit: 7/31/2024 Posts: 1560 Rating:
|
The only recommended way to backup a project is like said above using Project Duplicator. I've seen several situations in the past when copy/paste projects gave lots of troubles when trying to get your backup running on another machine. About a backup of a project in Runtime, you really don't need to buy an extra tool. I described a working way using a free, open source program called Hobocopy. You can find the old post and information here. This way is interesting for making regular backups while projects are running but after all it's still recommended to make a backup with Project Duplicator whenever the project can be stopped next time. |
Last edited by: SteBo at: 7/10/2013 10:27 AMLast edited by: SteBo at: 7/10/2013 10:27 AMLast edited by: SteBo at: 7/10/2013 7:33 AMB r g d s , |
|
This contribution was helpful to
2 thankful Users |
10/21/2019 9:07 PM | |
Posts: 3 Rating:
|
How do you save/copy WinCC projects while WinCC Runtime is running? the above file do not open. |
10/21/2019 9:11 PM | |
Posts: 3 Rating:
|
Dear, How to take a backup copy from wincc runtime when the project from wincc deleted by the programmer. thank you
|
Follow us on