1/7/2014 9:35 AM | |
Posts: 1368 Rating: (126) |
Hello Rollex, you have two networks (LAN A, LAN B) and want to connect each module (CPU and the 2 Server) to each network for redundancy? Without additional hardware, it is not possible to do that with a S7-300. You have to integrate the SCALANCE X204RNA (PRP) 6GK5204-0BA00-2KB2 On the Server, you need the SOFTNET IE RNA Software and two separate network cards. Look at this application http://support.automation.siemens.com/WW/view/de/78790945 Descripes this application your plan? Greetings, Pittiplatsch |
This contribution was helpful to1 thankful Users |
Follow us on