8/5/2021 2:33 PM | |
Joined: 3/17/2017 Last visit: 7/9/2024 Posts: 35 Rating: (2) |
Dear UMENCHO and other Experts, Can someone please tell me EXACTLY how can I switch an OP5-A1 unit (which has a project created and downloaded using COMTEXT already) into the Transfer mode for Upload? It's strange, but I can't follow recommendations from UMENCHO in this thread. I do have an OP5-A1 unit for testing. It did not have any data inside right out of the box. Someone has downloaded a project using COMTEXT into the unit and I'm now trying to Upload it (back to COMTEXT). But I can't do that, unless the OP5-A1 is in the right mode for it. Could someone tell me please how EXACTLY can I switch it? Thanks a lot in advance, s4gia ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 08/09/2021 08:14:40New subject after splitting |
|
9/2/2022 10:21 PM | |
Joined: 3/17/2017 Last visit: 7/9/2024 Posts: 35 Rating: (2) |
I managed to got the OP5 unit into the transfer mode and uploaded data. It took some time to figure out. |
9/3/2022 2:11 AM | |
Joined: 12/18/2014 Last visit: 7/12/2024 Posts: 33333 Rating: (4133) |
Here's a link to the manual of the OP5, OP15. Take a look at chapter 16. OP5, OP15 Operator Panel |
Follow us on