6/27/2018 11:02 AM | |
Joined: 12/12/2011 Last visit: 12/30/2020 Posts: 821 Rating: (40)
|
Hi, the ???? is only a placeholder. You need to configure your Danish controls etc. Regards M. |
Grundkurs/Systemkurs WinCC V7: |
|
7/2/2019 7:52 AM | |
Joined: 9/30/2016 Last visit: 5/23/2024 Posts: 912 Rating: (6) |
Hello Georg, Please also see the attached screenshots. I know it has been a while but I still haven't resolved this subject. As you can see in the screenshots - only English and Danish are chosen in the Text Library settings but in spite of that there is a LONG list of languages to choose from in the Graphics editor. How do I reduce that list to only English and Danish? If it is possible I would like the Graphics Editor to START with Danish in this project (so that the displays will show the Danish texts instead on question marks. On other projects the default should be English. I don't know if this is possible? As it is now I have to go into view and select the right language - every time I open the project - no matter if the project has used English or Danish texts.
AttachmentLang.zip (91 Downloads) |
Follow us on