3/18/2016 7:57 AM | |
Joined: 3/14/2008 Last visit: 7/12/2024 Posts: 2076 Rating: (930) |
Hi Rob, Take a look in WinCC explorer->Computer and right click your PC name on the right section and open Properties. Under tab: "Graphics Runtime", you can set your Windows attributes. For this, you want to have "Full screen". You can also determine which attributes you want to turn off, in section: "Turn off". The best way to shutdown WinCC is by the button: "Deactivate runtime" which is already present on the toolbar on the bottom of WinCC runtime. You may have to press the "Arrow" button just to change the buttonset. |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
Follow us on