10/31/2019 10:46 AM | |
Joined: 9/30/2016 Last visit: 5/23/2024 Posts: 912 Rating: (6) |
Please also see the attached screenshots. I have migrated a (small) project from WinCC 7.0 to WinCC7.4 Upd.1. When I open the project it shows the picture in too small a size and also without the buttons used to navigate between the pictures. How do I get it to open in the right size (the whole picture is filling the whole screen)? How do I get it to include the buttons? AttachmentWCC74.zip (64 Downloads) |
Follow us on