8/30/2019 9:00 AM | |
Joined: 5/20/2015 Last visit: 11/9/2024 Posts: 216 Rating: (3) |
Dear honorable Experts, I am using WinCC RT Advanced V14 SP1, how Can i Configure Modicon Modbus RTU driver for more than one device? in my case i have a PLC with single serial port and a Energy meter both are compatible on RS485 protocol and i already communicated with both devices but one by one, not both at a time. so my query is if WinCC RT Advanced have Modicon Modbus RTU driver then it should communicate with multiple devices just like any other modbus rtu driver, but there is no configuration environment in WinCC connection setting where i can add multiple slave devices, on same protocol. please guide me, and suggest any alternative if it is possible. regards Gabbar. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 08/30/2019 10:13:03New subject after splitting Last edited by: gabbar at: 08/30/2019 10:27:47Last edited by: gabbar at: 08/30/2019 10:35:30Last edited by: gabbar at: 08/30/2019 10:40:18Last edited by: gabbar at: 08/31/2019 07:45:34Let's do it... |
|
Follow us on