5/25/2023 6:43 PM | |
Joined: 9/28/2022 Last visit: 7/25/2024 Posts: 4 Rating: (0) |
I have similar request as well. How can that particular certificate generated by PLCSIM be added to the trusted root Certificate of the computer, as in this image. I would like to add it to the trusted root, but I am unable to locate it ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/26/2023 07:16:55New subject after splitting |
|
5/26/2023 8:39 AM | |
Joined: 5/6/2022 Last visit: 9/20/2024 Posts: 450 Rating: (90) |
Hi upsee, I have been looking for information and the only thing I found is the following: - This manual where the steps to be taken to use the certificates are discussed, which may be of interest to you: 'Using Certificates with TIA Portal' - Information about the 'Trusted Root Certification Authorities Certificate Store' on the Windows page. It can also clarify some of your doubts. |
If this Information really helps, you could use the Rate function |
|
5/26/2023 9:51 AM | |
Joined: 9/28/2022 Last visit: 7/25/2024 Posts: 4 Rating: (0) |
Hi ElonksuM_SN_BN Thank you for your response, I have indeed read through the Using Certificates with TIA Portal , I have added the certificates from the global security settings to the trusted certificate following the manual but I do not get the problem solved. From what I could observe, PLCSIM Advanced generates a completely new certificate when trying to run the instance of the CPU in PLCSIM, however, I can not locate this PLCSIM certificate anywhere in order to install it to the Trusted Certificates of the local PC. My concern is how to locate and install the PLCSIM generated certificate to the trusted certificate Thank you |
Follow us on