8/12/2011 1:32 PM | |
Posts: 37 Rating: (2) |
Dear All Can anybody tell how to estimate tags for any project? is ther any formula depending on Input output no? regards, Ninad |
10/18/2011 11:50 AM | |
Joined: 3/21/2006 Last visit: 10/7/2024 Posts: 10229 Rating: (1181) |
From Step7 project using a Tag Converting tool you can see estimated numbers of tags. Look to this link -> http://www.automation.siemens.com/microsite/wincc-flexible-easy/index_en.html --> experience --> Tag handling --> Importing tags. There are a "sample film" how to do this. But then also is possible to reduce their numbers words (group of bits) instead of bits...or internal tags (Is there really no limit to the number of internal tags in WinCC 7.0? ) Basically depending of the project the numbers are only expected in the moment when you build the project. Best regards, Hristo MIhalev |
This contribution was helpful to4 thankful Users |
5/8/2012 8:14 AM |
|
Joined: 11/18/2009 Last visit: 10/15/2024 Posts: 262 Rating: (18) |
I think this topic should be closed now. We can say that this topic is solved. |
5/14/2012 9:37 PM | |
Posts: 947 Rating: (45) |
necessary to consider for datalogging you can use is only available 1 or 2 or 4 byte variables |
Follow us on