9/16/2015 6:17 AM | |
Joined: 8/25/2006 Last visit: 7/30/2024 Posts: 2207 Rating:
|
Hello. 1. For Profibus DP-Master coupling there are two configurations: one is in the CPU and the other is in the SS52. 2. Yes, after replacing SS52, you need to load new or backup configuration. 3. *.pb5-files are ComProfibus files. You can open them via 'File-Open'. 4. You can find the cable pinout in the manual, chapter 3.5.3.11. Also you will find in this manual how to work with ComProfibus, how to load with SS52. Note, that you can also download configuration to SS52 via Profibus DP if your PC have DP-card (e.g. CP5511, CP5512, CP5611). |
This contribution was helpful to
1 thankful Users |
9/16/2015 2:09 PM | |
Joined: 8/25/2006 Last visit: 7/30/2024 Posts: 2207 Rating:
|
Hello. No, uploading from SS52 is not possible. |
Follow us on