4/17/2018 5:41 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating:
|
Please refer this Upload SIMOREG DC MASTER via routing thread for more information. |
This contribution was helpful to
1 thankful Users |
4/17/2018 8:24 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating:
|
Hello, Since your drive is in network & you need to communicate it via DriveES, please check your hardware project & check if drive is visible. Set up PG/PC parameters correctly so as to establish communication, then only you will be able upload or download parameters or check on line paraters. Please refer Upload SIMOREG DC MASTER via routing thread wherein expert Mr. KSN's reply, refer the manual which help you to set up the communication parameters. In the manual example is for Ethernet, but in your case, you need to set profibus related communication parameters. HTH. |
4/17/2018 9:03 AM | |
Joined: 8/25/2006 Last visit: 7/17/2024 Posts: 2207 Rating:
|
Hello. From your screen of installed software I don't see that you have installed DriveES Basic. You should have here 'Drive ES Basic Shared Components'. Then you need to configure your drive connected to PLC via Profibus in HWConfig, the drive should be inserted from DriveES HW profile. After that you will have your drive in Simatic Manager, insert 'Parameter set' in the folder 'Parameter' of the drive and open it via double-click. When DriveMonitor open it, you could change Online Settings via menu 'Tools' to Profibus DP. Look at screens in attachment. Attachmentscreen.zip (494 Downloads) |
This contribution was helpful to
3 thankful Users |
4/20/2018 2:17 AM | |
Posts: 31 Rating:
|
And yet-does not work. I used a PC-station. Installed software on the screenshoot. DC Simoreg is integrated into the project and is perfectly controlled by PLC. However, if I try to connect using DriveMonitor, an error occurs immediately.
AttachmentPrintScreen Files.zip (428 Downloads) |
4/26/2018 10:51 AM | |
Joined: 6/19/2017 Last visit: 6/28/2024 Posts: 8176 Rating:
|
New question published by ETTAHRIOUI is split to a separate thread with the subject Can change the MLFB on a simoreg Dc Master?. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on