6/10/2021 12:31 PM | |
Joined: 4/6/2021 Last visit: 6/3/2024 Posts: 32 Rating:
|
schufri thank you very much I have tried the steps and it works perfectly !!! This topic has been closed But before definitively leaving this method in the plant, I would like to test what it would be like to download from the simatic manager. Can you recommend me a document on how to do it? Actually I've already done it but it doesn't work ... at the engineering station I have managed to import the wincc project Then I try to download it to any of the servers either the master or the redundant one and the project is transferred but then when it tries to open it keeps showing the image1 and then the error of the image2 appears if I try to start the project manually it asks me to select a different path to reopen the project since the transferred project has been created in simatic manager. Do you know why this happens? I will open another topic regarding this problem with the simatic manager
AttachmentCamil.zip (122 Downloads) |
6/10/2021 2:35 PM | |
Joined: 10/10/2014 Last visit: 6/26/2024 Posts: 1725 Rating:
|
Hi c_khouri, Message: Database context does not exist or is invalid Cause: Open DB segments in the SQL server * Please check in the SQL Server Management Studio with the WinCC Explorer closed and closed runtime whether there are still open WinCC database segments. * Please also check the IP addresses of the network data. Also the order of the network types in the Simatic Shell * Please check the computer name and should not contain any special characters such as an underscore * Delete dcf file * Please also check the computer load. For configuration see: WinCC V7.5 SP1: Working with WinCC https://support.industry.siemens.com/cs/ww/en/view/109773058 16.1 Integration of WinCC in SIMATIC Manager Check also the isues form follow FAQ Which settings should you check if OS loading fails with PCS 7 or the OS project cannot be activated? https://support.industry.siemens.com/cs/ww/en/view/33123686 What are the requirements for operating SIMATIC WinCC in a Windows network? https://support.industry.siemens.com/cs/ww/en/view/868014 Best regards schufri |
Follow us on