4/13/2018 2:00 PM | |
Joined: 4/28/2015 Last visit: 9/9/2024 Posts: 3345 Rating: (379)
|
Hi, if you are using the Example Image V2.2 and the SDK V2.2 you will run into some compiler errors. The compiler erros are caused by not matching c++ versions of the SDK V2.2 and the Eclipse Plugin V1.2 (which suits to SDK V2.1.3). To avoid these errors:
After that the compiler errors are gone. Maybe you have to change something in the code (add a blank) and save the project before building the project again. Attached you can find a PDF with screenshots of the described steps. Best regards! AttachmentCompiler_Errors_V2.2.pdf (180 Downloads) |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
This contribution was helpful to4 thankful Users |
7/23/2018 7:42 AM | |
Joined: 4/28/2015 Last visit: 9/9/2024 Posts: 3345 Rating: (379)
|
HI, I just want to inform you that the Eclispe Plugin for the SDK version 2.2.0 is now online. With the Plugin V2.2 there is no need for the metioned adaptions. You can find it here. Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
This contribution was helpful to1 thankful Users |
Follow us on