12/6/2016 6:08 PM | |
Posts: 56 Rating:
|
Hello, When I am trying to open AS11 project in hardware configuration, it is giving error like "HW configuration (1230:2016)" "No changes can be made in this station". I tried open other projects as well but same issue I have found. Is it something related with user rights? I did the reinstallation of PCS7 V8.0 SP2 but same issue is appearing. \\ Ashish Wandhare HW Config is opened it displays "HW Config (1230:2016)" "No changes can be made in this station" AttachmentHW configration 400H.zip (441 Downloads) |
12/7/2016 7:22 AM | |
Posts: 56 Rating:
|
Hello RugbyGuy, Thanks a lot for your reply. -Yes I checked that & both look same. See attached screenshot. -Yes that is quite strange, some normal CPU's I can see tin HW Config Catalog but not 410-5H,412-3H,412-5H,414-5H,415-5H & 416-5H & in project I am using 416-5H. I rebuild the machine from scratch & installed PCS7. - I have attached screenshot for the same as well & checked the description of error looks okay to me. //Ashish Wandhare AttachmentInstalled software on Project computer.zip (399 Downloads) |
12/7/2016 10:20 AM | |
Posts: 56 Rating:
|
Hello, To resolve the issue I have installed latest HSP in Hardware configuration from below web link & it works. https://support.industry.siemens.com/cs/document/23183356/step-7-v5-x-hardware-support-packages-(hsps-as-at-11-2016)-for-installing-hardware-updates-in-the-hardware-configuration?dti=0&lc=en-WW Thanks a lot for help. //Ashish Wandhare AttachmentHSP Instruction.pdf (581 Downloads) |
This contribution was helpful to
1 thankful Users |
12/7/2016 11:13 AM | |
Joined: 3/14/2008 Last visit: 7/2/2024 Posts: 2075 Rating:
|
Hi, Make sure you only install HSP's which are released for your PCS7 version. Step7 is something else than PCS7 although it is the basis of PCS7. |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on