6/15/2010 5:25 AM | |
Posts: 16 Rating: (0) |
Hi, I am lacking the WinCC Component Object Manager package, and I can't find this option when installing WinCC. Please help, thanks. Splitted from wincc integration. |
Last edited by: O_Moderator at: 6/15/2010 12:36 PMnew subject after splitting |
|
6/15/2010 7:31 AM | |
Joined: 3/21/2006 Last visit: 10/7/2024 Posts: 10229 Rating: (1181) |
Hello, Look at http://support.automation.siemens.com/WW/view/en/11841504 Perhaps will helps you. Best regards, Hristo Mihalev |
This contribution was helpful to1 thankful Users |
6/15/2010 9:14 AM | |
Joined: 9/6/2008 Last visit: 5/7/2022 Posts: 1121 Rating: (86) |
Hi Bobby007 During installation you have to select user defined installation (Please find the attachment), then you have to follow the link that umencho has given. have fun... Attachmentinstallationw.zip (3894 Downloads) |
Jazz |
|
This contribution was helpful to1 thankful Users |
6/16/2010 9:05 AM | |
Joined: 1/4/2010 Last visit: 9/25/2024 Posts: 650 Rating: (40)
|
Hi You should install Step 7 v5.4 SP4 see the attached compatibility list: http://support.automation.siemens.com/WW/view/de/21927773 Please have a look in WinCC Explorer > Help > WinCC Explorer Help Here you see the installed SW and I think you see that the object manager is installed. |
Last edited by: Romulus at: 6/16/2010 9:53 AMRegards |
|
This contribution was helpful to1 thankful Users |
1/18/2018 8:38 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
New question published by M_FA is split to a separate thread with the subject Error while installing Object Manager. Best regards |
Follow us on