8/27/2017 3:37 PM | |
Posts: 4 Rating: (0) |
Dear Sir, In our kampf alitter we have s5-135u, and simadyn d. Our complete system looks healthy. In s5 there are 2 cp524 cards. One cp 524 communicates directly to scada through rs 432 and the 2nd cp 524 communicates with the simadyn d through a tty card. We have healthy communication between scada and s5 but we are unable to get communication between simadyn d and s5. We have changed the ss4 and ss1 card in the simadyn d. But are now doubting the cp524 and tty. We need an expert who can verify the s5 healthiness and use a com5 software to communicate with the cp524 through the tty card. ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 8/28/2017 9:57:50 AMNew subject after splitting |
|
8/29/2017 2:18 AM | |
Posts: 3093 Rating: (323) |
Hello HD4264, Regards, |
This contribution was helpful to1 thankful Users |
9/18/2017 5:10 PM | |
Posts: 4 Rating: (0) |
Protocol Is TTY. We are getting pafe error for send all and recv all. |
9/18/2017 5:47 PM | |
Posts: 3093 Rating: (323) |
Hello, Well, and which PAFE do you get? Manual CP524 volume 2 Regards, |
Last edited by: Kaulquappe at: 9/18/2017 6:13:07 PMLink added Last edited by: Kaulquappe at: 9/18/2017 6:15:40 PMLast edited by: Kaulquappe at: 9/18/2017 6:18:15 PM |
|
9/19/2017 7:36 AM | |
Posts: 4 Rating: (0) |
Yes. It is Rk512 & pro. 3964r. And Get error of send all and receive all. |
9/21/2017 7:39 AM | |
Joined: 8/25/2006 Last visit: 9/13/2024 Posts: 2209 Rating: (278) |
Hello. At which FB you have this error? @CSD03? Show also configuration of CRV/CTV blocks. |
Follow us on