6/19/2024 8:59 AM | |
Joined: 1/21/2013 Last visit: 8/1/2024 Posts: 3043 Rating:
|
Hi MedHabib, I would recommend that you use the TIA Selection Tool cloud and specify the type of axes you want to use. That will give you a rough estimate. It is not only important to know how many axes you are planning. It is also important to know how they will be controlled. A drive-controlled axis, such as a SINAMICS S120, will require less performance from the PLC than a PLC-controlled axis. To configure your motion requirements in TIA Selection Tool cloud select Catalog > Controllers > S7-1500. There, under Special product properties > CPU design, enable motion control to enable the motion configuration. Kind regards |
6/19/2024 9:21 AM | |
Joined: 4/22/2024 Last visit: 8/2/2024 Posts: 11 Rating:
|
I have used drives from another brand and integrated their GSD files into TIA Portal. How can this be verified? |
6/19/2024 9:38 AM | |
Joined: 1/21/2013 Last visit: 8/1/2024 Posts: 3043 Rating:
|
Hi MedHabib, Even with third-party axes, it is important to know who is doing the position control. Is it the PLC or the drive? However, since the wrong choice will result in additional costs and lost time, it is better to contact Siemens Technical Consulting. Kind regards |
Follow us on