6/22/2022 1:54 PM | |
Joined: 4/21/2021 Last visit: 3/21/2023 Posts: 45 Rating: (0) |
Hello, I order SIMATIC WinCC Runtime Professional V15.1 (6AV2105-0HA05-0AH0) When I received the installable file, I found at the software: 1- SIMATIC_WinCC_Runtime_Professional_V15_1 2- SIMATIC_NET_PC_Software_V15_SP1 1- Do I need to install the second software (SIMATIC_NET_PC_Software_V15_SP1) to establish profinet communication between IPC547G and CPU 1515-2PN? 2- In my architecture I used IE general in profinet communication between IPC547G (6AG4104-4JA12-1EC1) and CPU 1515-2PN, In this case the communication is possible if we use the standard network card of IPC547G (6AG4104-4JA12- 1EC1)? see IPC547G caractéristic in attachement Thankyou for help, AttachmentIPC547G caractéristic.pdf (350 Downloads) |
Follow us on