11/9/2021 12:52 PM | |
Joined: 10/19/2021 Last visit: 9/9/2022 Posts: 2 Rating:
|
Hello. I have the same problem - IE General remains in STOP mode after I inserted it in Station Configurator. I need to configure OPC Server by OPC SimaticNET. To do that I added first IE General in slot 2 then I added OPC Server in slot 3. After that IE General is in STOP mode even after I restart OS. Diagnostic messages from Station Configurator are following: 2 !! 09.11.2021 11:21:09 Router The CP with index 2 is not operational! Error 0x0381 occurred. 1 09.11.2021 11:21:08 IE-Converter Index 2: The module was reconfigured according to the defined configuration. I have Windows Server 2016 Standart and SIMATIC NET 14 SP1. All licenses are already installed. I plan to use XDB file, which I configured from Step 7 5.5 SP4 (on another computer). The only way to make IE General work in RUN is to Import XDB file, then remove IE General from Station Configurator and insert it again. After that IE General work in RUN mode. But it does not make sence. Please take me a hint how to make this soft work. Thanks in advance ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/10/2021 09:26:05New subject after splitting |
|
Follow us on