6/3/2013 10:05 AM | |
Joined: 8/25/2006 Last visit: 10/18/2024 Posts: 2209 Rating: (279) |
Hello. Lookhere.
|
6/3/2013 10:38 AM | |
Posts: 72 Rating: (2) |
hello KSN thanks for your replay it support 6ES7 155-6AU00-0BN0 but i need6ES7 155-6AA00-0BN0 booth are same ?
|
6/3/2013 10:48 AM | |
Joined: 8/25/2006 Last visit: 10/18/2024 Posts: 2209 Rating: (279) |
Hello. I'm not 100% sure, but it seems they are different only inbus adapter 2xRJ45included in 6es7155-6aa0.
|
2/11/2016 10:32 AM | |
Posts: 7 Rating: (0) |
hiExperts, I need GSD file IM 155 - 6 PN HF ET200SP (6ES7 155-6AU00-0CN0) from where i will get ? I'm using simatic manager V5.5 sp4. Best Regards Fitri Aminula |
2/11/2016 11:44 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1054) |
hi Fitri Aminula, see the Delivery Release of the Device: New Components for ET 200SP Released for Delivery (I/O Modules: analog high-speed modules, interface modules, power metering module) and accessoriesThere you find a Link where you can download the GSD-Files.PROFINET GSD files : ET 200SPYou need minimum Step7 5.5 SP4 HF1.HF8 for Step7 5.5 SP4 can be downloaded here:Download from Hotfix 8 to STEP 7 V5.5 SP4 and STEP 7 Professional 2010 SR4hope this helps,regards, |
FCK WAR! |
|
Follow us on