Industry Online Support
Technical Forum
6/4/2011 6:26 PM | |
Posts: 30 Rating: (0) |
Dear Expert's, We have IM151-8 3PN/DP CPU, first port is used for communication with IM at remote area and the second is connected to work station(Computer) for SCADA, see PDF. now we want to add one more work station so as we think the requirement to do this are: one ethernet switch, ethernet cable, computer, Wincc Flexible runtime software with key but in PDF one more card is show (1612 A2 PCI card) so my doubt is about this card, is it needed??? I think we can direct connect ethernet cable between ethernet switch and lan port of computer, am i right? thnks naveen Attachment01_SC.pdf (65 Downloads) |
Last edited by: Naveen Paliwal at: 6/4/2011 6:28 PM |
|
6/4/2011 10:05 PM | |
Posts: 947 Rating: (45) |
IM151-8 is equivalent 314CPU with integrate Profinet. Therefore I do not see any problem to connect it to SCADA |
Follow us on