1/26/2021 4:19 PM | |
Joined: 10/10/2005 Last visit: 4/18/2024 Posts: 1917 Rating: (132) |
Hello Dinesh, the settings in the PG/PC interface is dependent on the driver which is installed in your PC, example "Intel(R) Centrino (R) Advanced-N 62…". Please see the instruction of the FAQ: How do you generally parameterize the PG/PC interface and how do you ensure that the device driver can be selected and is visible? With best regards |
Last edited by: Cicero at: 01/26/2021 16:20:37 |
|
1/26/2021 5:16 PM | |
Joined: 1/17/2020 Last visit: 5/11/2024 Posts: 46 Rating: (6) |
Hi 1. Online firmware update via STEP7 HW Config:
The download process is not visible on the IM153-2. After successful download, the new firmware can be started automatically or with power off/on. 2. Online firmware update via SIMATIC Manager:
The download process is not visible on the IM153-2. After successful download, the new firmware can be started automatically or with power off/on. |
Rate please if it was useful! |
|
Follow us on